AXIS#.GEAR.IN

Description

This parameter sets the denominator of the gear ratio for the electronic gearing mode. The gear ratio is used to increase and decrease the slave velocity. The slave velocity is calculated by the following formula:

Slave velocity = Master velocity * AXIS#.GEAR.OUT/AXIS#.GEAR.IN

Be sure the external master source number of signals per revolution is set correctly. See AXIS#.GEAR.FBSOURCE to determine the gearing master source and verify the feedback resolution for that device.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

1 to 65,535

Default Value

1

Data Type

Integer

See Also

N/A

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.GEAR.IN

5006h

03h

Unsigned16

-

-

Read/Write

No

AXIS2.GEAR.IN

5106h

03h

Unsigned16

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.GEAR.IN

5502

157E

Unsigned16

Read/Write

-

AXIS2.GEAR.IN

71038

1157

Unsigned16

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.GEAR.IN

5502

Unsigned16

Read/Write

-